多个设备
- Box measurement 应用,来自多个不同视角的多个摄像头可以提供更好的尺寸估算
- People counter/tracker 应用,多个摄像头可以统计/跟踪大区域内的人员(例如购物中心)
- 将多个摄像头安装在机器人的前/后/左/右侧,实现全 360° 视野,这样您的机器人就可以感知周围的整个区域,而无论其位置如何。
演示

Command Line
1Connected to 18443010F105060F00
2 >>> MXID: 18443010F105060F00
3 >>> Num of cameras: 3
4 >>> USB speed: UsbSpeed.SUPER
5 >>> Board name: DM9098
6 >>> Product name: OAK-D S2 FF
7 Connected to 1844301011F4C51200
8 >>> MXID: 1844301011F4C51200
9 >>> Num of cameras: 3
10 >>> USB speed: UsbSpeed.UNKNOWN
11 >>> Board name: NG9097
12 >>> Product name: OAK-D Pro PoE AF设置
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5import contextlib
6
7def createPipeline():
8 # Start defining a pipeline
9 pipeline = dai.Pipeline()
10 # Define a source - color camera
11 camRgb = pipeline.create(dai.node.ColorCamera)
12
13 camRgb.setPreviewSize(300, 300)
14 camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
15 camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
16 camRgb.setInterleaved(False)
17
18 # Create output
19 xoutRgb = pipeline.create(dai.node.XLinkOut)
20 xoutRgb.setStreamName("rgb")
21 camRgb.preview.link(xoutRgb.input)
22
23 return pipeline
24
25
26with contextlib.ExitStack() as stack:
27 deviceInfos = dai.Device.getAllAvailableDevices()
28 usbSpeed = dai.UsbSpeed.SUPER
29 openVinoVersion = dai.OpenVINO.Version.VERSION_2021_4
30
31 qRgbMap = []
32 devices = []
33
34 for deviceInfo in deviceInfos:
35 deviceInfo: dai.DeviceInfo
36 device: dai.Device = stack.enter_context(dai.Device(openVinoVersion, deviceInfo, usbSpeed))
37 devices.append(device)
38 print("===Connected to ", deviceInfo.getMxId())
39 mxId = device.getMxId()
40 cameras = device.getConnectedCameras()
41 usbSpeed = device.getUsbSpeed()
42 eepromData = device.readCalibration2().getEepromData()
43 print(" >>> MXID:", mxId)
44 print(" >>> Num of cameras:", len(cameras))
45 print(" >>> USB speed:", usbSpeed)
46 if eepromData.boardName != "":
47 print(" >>> Board name:", eepromData.boardName)
48 if eepromData.productName != "":
49 print(" >>> Product name:", eepromData.productName)
50
51 pipeline = createPipeline()
52 device.startPipeline(pipeline)
53
54 # Output queue will be used to get the rgb frames from the output defined above
55 q_rgb = device.getOutputQueue(name="rgb", maxSize=4, blocking=False)
56 stream_name = "rgb-" + mxId + "-" + eepromData.productName
57 qRgbMap.append((q_rgb, stream_name))
58
59 while True:
60 for q_rgb, stream_name in qRgbMap:
61 if q_rgb.has():
62 cv2.imshow(stream_name, q_rgb.get().getCvFrame())
63
64 if cv2.waitKey(1) == ord('q'):
65 breakPipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。