旋转 OAK 上的空间检测
camRgb.setImageOrientation(dai.CameraImageOrientation.ROTATE_180_DEG)。 这意味着节点的所有输出(still/isp/video/preview)都将已旋转。我们旋转 depth 帧,在 StereoDepth 创建它们之后。有人可能会尝试在将单声道帧发送到 StereoDepth 节点之前旋转它们,但这不起作用,因为立体校准需要反映这些更改。因此,我们使用 ImageManip 节点来旋转 depth(下面的代码),然后将其发送到 MobileNetSpatialDetectionNetwork。Command Line
1manip = pipeline.createImageManip()
2 # Vertical + Horizontal flip == rotate frame for 180°
3 manip.initialConfig.setVerticalFlip(True)
4 manip.initialConfig.setHorizontalFlip(True)
5 manip.setFrameType(dai.ImgFrame.Type.RAW16)
6 stereo.depth.link(manip.inputImage)类似示例:
- RGB & MobilenetSSD with spatial data
- Spatial object tracker on RGB
- Mono & MobilenetSSD with spatial data
- RGB & TinyYolo with spatial data
设置
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3from pathlib import Path
4import sys
5import cv2
6import depthai as dai
7import numpy as np
8'''
9Spatial object detections demo for 180° rotated OAK camera.
10'''
11
12# Get argument first
13nnBlobPath = str((Path(__file__).parent / Path('../models/mobilenet-ssd_openvino_2021.4_6shave.blob')).resolve().absolute())
14if len(sys.argv) > 1:
15 nnBlobPath = sys.argv[1]
16
17if not Path(nnBlobPath).exists():
18 import sys
19 raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"')
20
21# MobilenetSSD label texts
22labelMap = ["background", "aeroplane", "bicycle", "bird", "boat", "bottle", "bus", "car", "cat", "chair", "cow",
23 "diningtable", "dog", "horse", "motorbike", "person", "pottedplant", "sheep", "sofa", "train", "tvmonitor"]
24
25syncNN = True
26
27# Create pipeline
28pipeline = dai.Pipeline()
29
30# Define sources and outputs
31camRgb = pipeline.createColorCamera()
32spatialDetectionNetwork = pipeline.create(dai.node.MobileNetSpatialDetectionNetwork)
33monoLeft = pipeline.create(dai.node.MonoCamera)
34monoRight = pipeline.create(dai.node.MonoCamera)
35stereo = pipeline.create(dai.node.StereoDepth)
36
37xoutRgb = pipeline.create(dai.node.XLinkOut)
38xoutNN = pipeline.create(dai.node.XLinkOut)
39xoutDepth = pipeline.create(dai.node.XLinkOut)
40
41xoutRgb.setStreamName("rgb")
42xoutNN.setStreamName("detections")
43xoutDepth.setStreamName("depth")
44
45# Properties
46camRgb.setPreviewSize(300, 300)
47camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
48camRgb.setInterleaved(False)
49camRgb.setColorOrder(dai.ColorCameraProperties.ColorOrder.BGR)
50camRgb.setImageOrientation(dai.CameraImageOrientation.ROTATE_180_DEG)
51
52monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
53monoLeft.setCamera("left")
54monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
55monoRight.setCamera("right")
56
57# Setting node configs
58stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
59# Align depth map to the perspective of RGB camera, on which inference is done
60stereo.setDepthAlign(dai.CameraBoardSocket.CAM_A)
61stereo.setSubpixel(True)
62stereo.setOutputSize(monoLeft.getResolutionWidth(), monoLeft.getResolutionHeight())
63
64rotate_stereo_manip = pipeline.createImageManip()
65rotate_stereo_manip.initialConfig.setVerticalFlip(True)
66rotate_stereo_manip.initialConfig.setHorizontalFlip(True)
67rotate_stereo_manip.setFrameType(dai.ImgFrame.Type.RAW16)
68stereo.depth.link(rotate_stereo_manip.inputImage)
69
70spatialDetectionNetwork.setBlobPath(nnBlobPath)
71spatialDetectionNetwork.setConfidenceThreshold(0.5)
72spatialDetectionNetwork.input.setBlocking(False)
73spatialDetectionNetwork.setBoundingBoxScaleFactor(0.5)
74spatialDetectionNetwork.setDepthLowerThreshold(100)
75spatialDetectionNetwork.setDepthUpperThreshold(5000)
76
77# Linking
78monoLeft.out.link(stereo.left)
79monoRight.out.link(stereo.right)
80
81camRgb.preview.link(spatialDetectionNetwork.input)
82if syncNN:
83 spatialDetectionNetwork.passthrough.link(xoutRgb.input)
84else:
85 camRgb.preview.link(xoutRgb.input)
86
87spatialDetectionNetwork.out.link(xoutNN.input)
88
89rotate_stereo_manip.out.link(spatialDetectionNetwork.inputDepth)
90spatialDetectionNetwork.passthroughDepth.link(xoutDepth.input)
91color = (255, 0, 0)
92# Connect to device and start pipeline
93with dai.Device(pipeline) as device:
94
95 # Output queues will be used to get the rgb frames and nn data from the outputs defined above
96 previewQueue = device.getOutputQueue(name="rgb", maxSize=4, blocking=False)
97 detectionNNQueue = device.getOutputQueue(name="detections", maxSize=4, blocking=False)
98 depthQueue = device.getOutputQueue(name="depth", maxSize=4, blocking=False)
99
100 while True:
101 inPreview = previewQueue.get()
102 inDet = detectionNNQueue.get()
103 depth = depthQueue.get()
104
105 frame = inPreview.getCvFrame()
106 depthFrame = depth.getFrame() # depthFrame values are in millimeters
107
108 depth_downscaled = depthFrame[::4]
109 if np.all(depth_downscaled == 0):
110 min_depth = 0 # Set a default minimum depth value when all elements are zero
111 else:
112 min_depth = np.percentile(depth_downscaled[depth_downscaled != 0], 1)
113 max_depth = np.percentile(depth_downscaled, 99)
114 depthFrameColor = np.interp(depthFrame, (min_depth, max_depth), (0, 255)).astype(np.uint8)
115 depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_HOT)
116
117 detections = inDet.detections
118
119 # If the frame is available, draw bounding boxes on it and show the frame
120 height = frame.shape[0]
121 width = frame.shape[1]
122 for detection in detections:
123 roiData = detection.boundingBoxMapping
124 roi = roiData.roi
125 roi = roi.denormalize(depthFrameColor.shape[1], depthFrameColor.shape[0])
126 topLeft = roi.topLeft()
127 bottomRight = roi.bottomRight()
128 xmin = int(topLeft.x)
129 ymin = int(topLeft.y)
130 xmax = int(bottomRight.x)
131 ymax = int(bottomRight.y)
132 cv2.rectangle(depthFrameColor, (xmin, ymin), (xmax, ymax), color, cv2.FONT_HERSHEY_SCRIPT_SIMPLEX)
133
134 # Denormalize bounding box
135 x1 = int(detection.xmin * width)
136 x2 = int(detection.xmax * width)
137 y1 = int(detection.ymin * height)
138 y2 = int(detection.ymax * height)
139 try:
140 label = labelMap[detection.label]
141 except:
142 label = detection.label
143 cv2.putText(frame, str(label), (x1 + 10, y1 + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
144 cv2.putText(frame, "{:.2f}".format(detection.confidence*100), (x1 + 10, y1 + 35), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
145 cv2.putText(frame, f"X: {int(detection.spatialCoordinates.x)} mm", (x1 + 10, y1 + 50), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
146 cv2.putText(frame, f"Y: {int(detection.spatialCoordinates.y)} mm", (x1 + 10, y1 + 65), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
147 cv2.putText(frame, f"Z: {int(detection.spatialCoordinates.z)} mm", (x1 + 10, y1 + 80), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
148
149 cv2.rectangle(frame, (x1, y1), (x2, y2), (255, 0, 0), cv2.FONT_HERSHEY_SIMPLEX)
150
151 cv2.imshow("depth", depthFrameColor)
152 cv2.imshow("preview", frame)
153
154 if cv2.waitKey(1) == ord('q'):
155 breakPipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。