深度裁剪控制
w向上移动裁剪区域a向左移动裁剪区域s向下移动裁剪区域d向右移动裁剪区域
类似示例:
演示
设置
源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3"""
4This example shows usage of depth camera in crop mode with the possibility to move the crop.
5Use 'WASD' in order to do it.
6"""
7
8import cv2
9import depthai as dai
10import numpy as np
11
12# Step size ('W','A','S','D' controls)
13stepSize = 0.02
14
15# Create pipeline
16pipeline = dai.Pipeline()
17
18# Define sources and outputs
19monoRight = pipeline.create(dai.node.MonoCamera)
20monoLeft = pipeline.create(dai.node.MonoCamera)
21manip = pipeline.create(dai.node.ImageManip)
22stereo = pipeline.create(dai.node.StereoDepth)
23
24configIn = pipeline.create(dai.node.XLinkIn)
25xout = pipeline.create(dai.node.XLinkOut)
26
27configIn.setStreamName('config')
28xout.setStreamName("depth")
29
30# Crop range
31topLeft = dai.Point2f(0.2, 0.2)
32bottomRight = dai.Point2f(0.8, 0.8)
33
34# Properties
35monoRight.setCamera("right")
36monoLeft.setCamera("left")
37monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
38monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
39
40manip.initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
41manip.setMaxOutputFrameSize(monoRight.getResolutionHeight()*monoRight.getResolutionWidth()*3)
42stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
43stereo.setSubpixel(True)
44
45# Linking
46configIn.out.link(manip.inputConfig)
47stereo.depth.link(manip.inputImage)
48manip.out.link(xout.input)
49monoRight.out.link(stereo.right)
50monoLeft.out.link(stereo.left)
51
52# Connect to device and start pipeline
53with dai.Device(pipeline) as device:
54
55 # Queues
56 q = device.getOutputQueue(xout.getStreamName(), maxSize=4, blocking=False)
57 configQueue = device.getInputQueue(configIn.getStreamName())
58
59 sendCamConfig = False
60
61 while True:
62 inDepth = q.get()
63 depthFrame = inDepth.getFrame() # depthFrame values are in millimeters
64
65 # Frame is transformed, the color map will be applied to highlight the depth info
66 depth_downscaled = depthFrame[::4]
67 if np.all(depth_downscaled == 0):
68 min_depth = 0 # Set a default minimum depth value when all elements are zero
69 else:
70 min_depth = np.percentile(depth_downscaled[depth_downscaled != 0], 1)
71 max_depth = np.percentile(depth_downscaled, 99)
72 depthFrameColor = np.interp(depthFrame, (min_depth, max_depth), (0, 255)).astype(np.uint8)
73 depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_HOT)
74
75 # Frame is ready to be shown
76 cv2.imshow("depth", depthFrameColor)
77
78 # Update screen
79 key = cv2.waitKey(10)
80 if key == ord('q'):
81 break
82 elif key == ord('w'):
83 if topLeft.y - stepSize >= 0:
84 topLeft.y -= stepSize
85 bottomRight.y -= stepSize
86 sendCamConfig = True
87 elif key == ord('a'):
88 if topLeft.x - stepSize >= 0:
89 topLeft.x -= stepSize
90 bottomRight.x -= stepSize
91 sendCamConfig = True
92 elif key == ord('s'):
93 if bottomRight.y + stepSize <= 1:
94 topLeft.y += stepSize
95 bottomRight.y += stepSize
96 sendCamConfig = True
97 elif key == ord('d'):
98 if bottomRight.x + stepSize <= 1:
99 topLeft.x += stepSize
100 bottomRight.x += stepSize
101 sendCamConfig = True
102
103 # Send new config to camera
104 if sendCamConfig:
105 cfg = dai.ImageManipConfig()
106 cfg.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
107 configQueue.send(cfg)
108 sendCamConfig = False流程图
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。