UVC & Color Camera
cv2.VideoCapture(), native camera apps, and more.Similar samples:
Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pyCode used for testing
Python
1import cv2
2
3# Initialize the VideoCapture object to use the default camera (camera index 0 is webcam)
4cap = cv2.VideoCapture(1)
5
6# Check if the camera opened successfully
7if not cap.isOpened():
8 print("Error: Could not open camera.")
9 exit()
10
11# Loop to continuously get frames from the camera
12while True:
13 ret, frame = cap.read()
14
15 if not ret:
16 print("Error: Could not read frame.")
17 break
18
19 cv2.imshow('Video Feed', frame)
20
21 if cv2.waitKey(1) & 0xFF == ord('q'):
22 break
23
24cap.release()
25cv2.destroyAllWindows()Source code
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import time
4import argparse
5
6parser = argparse.ArgumentParser()
7parser.add_argument('-fb', '--flash-bootloader', default=False, action="store_true")
8parser.add_argument('-f', '--flash-app', default=False, action="store_true")
9parser.add_argument('-l', '--load-and-exit', default=False, action="store_true")
10args = parser.parse_args()
11
12if args.load_and_exit:
13 import os
14 # Disabling device watchdog, so it doesn't need the host to ping periodically.
15 # Note: this is done before importing `depthai`
16 os.environ["DEPTHAI_WATCHDOG"] = "0"
17
18import depthai as dai
19
20def getPipeline():
21 enable_4k = False # Will downscale 4K -> 1080p
22
23 pipeline = dai.Pipeline()
24
25 # Define a source - color camera
26 cam_rgb = pipeline.createColorCamera()
27 cam_rgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
28 cam_rgb.setInterleaved(False)
29 #cam_rgb.initialControl.setManualFocus(130)
30
31 if enable_4k:
32 cam_rgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_4_K)
33 cam_rgb.setIspScale(1, 2)
34 else:
35 cam_rgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
36
37 # Create an UVC (USB Video Class) output node
38 uvc = pipeline.createUVC()
39 cam_rgb.video.link(uvc.input)
40
41 # Note: if the pipeline is sent later to device (using startPipeline()),
42 # it is important to pass the device config separately when creating the device
43 config = dai.Device.Config()
44 # config.board.uvc = dai.BoardConfig.UVC() # enable default 1920x1080 NV12
45 config.board.uvc = dai.BoardConfig.UVC(1920, 1080)
46 config.board.uvc.frameType = dai.ImgFrame.Type.NV12
47 # config.board.uvc.cameraName = "My Custom Cam"
48 pipeline.setBoardConfig(config.board)
49
50 return pipeline
51
52# Will flash the bootloader if no pipeline is provided as argument
53def flash(pipeline=None):
54 (f, bl) = dai.DeviceBootloader.getFirstAvailableDevice()
55 bootloader = dai.DeviceBootloader(bl, True)
56
57 # Create a progress callback lambda
58 progress = lambda p : print(f'Flashing progress: {p*100:.1f}%')
59
60 startTime = time.monotonic()
61 if pipeline is None:
62 print("Flashing bootloader...")
63 bootloader.flashBootloader(progress)
64 else:
65 print("Flashing application pipeline...")
66 bootloader.flash(progress, pipeline)
67
68 elapsedTime = round(time.monotonic() - startTime, 2)
69 print("Done in", elapsedTime, "seconds")
70
71if args.flash_bootloader or args.flash_app:
72 if args.flash_bootloader: flash()
73 if args.flash_app: flash(getPipeline())
74 print("Flashing successful. Please power-cycle the device")
75 quit()
76
77if args.load_and_exit:
78 device = dai.Device(getPipeline())
79 print("\nDevice started. Attempting to force-terminate this process...")
80 print("Open an UVC viewer to check the camera stream.")
81 print("To reconnect with depthai, a device power-cycle may be required in some cases")
82 # We do not want the device to be closed, so terminate the process uncleanly.
83 # (TODO add depthai API to be able to cleanly exit without closing device)
84 import signal
85 os.kill(os.getpid(), signal.SIGTERM)
86
87# Standard UVC load with depthai
88with dai.Device(getPipeline()) as device:
89 print("\nDevice started, please keep this process running")
90 print("and open an UVC viewer to check the camera stream.")
91 print("\nTo close: Ctrl+C")
92
93 # Doing nothing here, just keeping the host feeding the watchdog
94 while True:
95 try:
96 time.sleep(0.1)
97 except KeyboardInterrupt:
98 breakPipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。