空间位置计算器
类似示例:
演示

设置
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5import numpy as np
6stepSize = 0.05
7
8newConfig = False
9
10# Create pipeline
11pipeline = dai.Pipeline()
12
13# Define sources and outputs
14monoLeft = pipeline.create(dai.node.MonoCamera)
15monoRight = pipeline.create(dai.node.MonoCamera)
16stereo = pipeline.create(dai.node.StereoDepth)
17spatialLocationCalculator = pipeline.create(dai.node.SpatialLocationCalculator)
18
19xoutDepth = pipeline.create(dai.node.XLinkOut)
20xoutSpatialData = pipeline.create(dai.node.XLinkOut)
21xinSpatialCalcConfig = pipeline.create(dai.node.XLinkIn)
22
23xoutDepth.setStreamName("depth")
24xoutSpatialData.setStreamName("spatialData")
25xinSpatialCalcConfig.setStreamName("spatialCalcConfig")
26
27# Properties
28monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
29monoLeft.setCamera("left")
30monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
31monoRight.setCamera("right")
32
33stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
34stereo.setLeftRightCheck(True)
35stereo.setSubpixel(True)
36
37# Config
38topLeft = dai.Point2f(0.4, 0.4)
39bottomRight = dai.Point2f(0.6, 0.6)
40
41config = dai.SpatialLocationCalculatorConfigData()
42config.depthThresholds.lowerThreshold = 100
43config.depthThresholds.upperThreshold = 10000
44calculationAlgorithm = dai.SpatialLocationCalculatorAlgorithm.MEDIAN
45config.roi = dai.Rect(topLeft, bottomRight)
46
47spatialLocationCalculator.inputConfig.setWaitForMessage(False)
48spatialLocationCalculator.initialConfig.addROI(config)
49
50# Linking
51monoLeft.out.link(stereo.left)
52monoRight.out.link(stereo.right)
53
54spatialLocationCalculator.passthroughDepth.link(xoutDepth.input)
55stereo.depth.link(spatialLocationCalculator.inputDepth)
56
57spatialLocationCalculator.out.link(xoutSpatialData.input)
58xinSpatialCalcConfig.out.link(spatialLocationCalculator.inputConfig)
59
60# Connect to device and start pipeline
61with dai.Device(pipeline) as device:
62
63 # Output queue will be used to get the depth frames from the outputs defined above
64 depthQueue = device.getOutputQueue(name="depth", maxSize=4, blocking=False)
65 spatialCalcQueue = device.getOutputQueue(name="spatialData", maxSize=4, blocking=False)
66 spatialCalcConfigInQueue = device.getInputQueue("spatialCalcConfig")
67
68 color = (255, 255, 255)
69
70 print("Use WASD keys to move ROI!")
71
72 while True:
73 inDepth = depthQueue.get() # Blocking call, will wait until a new data has arrived
74
75 depthFrame = inDepth.getFrame() # depthFrame values are in millimeters
76
77 depth_downscaled = depthFrame[::4]
78 if np.all(depth_downscaled == 0):
79 min_depth = 0 # Set a default minimum depth value when all elements are zero
80 else:
81 min_depth = np.percentile(depth_downscaled[depth_downscaled != 0], 1)
82 max_depth = np.percentile(depth_downscaled, 99)
83 depthFrameColor = np.interp(depthFrame, (min_depth, max_depth), (0, 255)).astype(np.uint8)
84 depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_HOT)
85
86 spatialData = spatialCalcQueue.get().getSpatialLocations()
87 for depthData in spatialData:
88 roi = depthData.config.roi
89 roi = roi.denormalize(width=depthFrameColor.shape[1], height=depthFrameColor.shape[0])
90 xmin = int(roi.topLeft().x)
91 ymin = int(roi.topLeft().y)
92 xmax = int(roi.bottomRight().x)
93 ymax = int(roi.bottomRight().y)
94
95 depthMin = depthData.depthMin
96 depthMax = depthData.depthMax
97
98 fontType = cv2.FONT_HERSHEY_TRIPLEX
99 cv2.rectangle(depthFrameColor, (xmin, ymin), (xmax, ymax), color, 1)
100 cv2.putText(depthFrameColor, f"X: {int(depthData.spatialCoordinates.x)} mm", (xmin + 10, ymin + 20), fontType, 0.5, color)
101 cv2.putText(depthFrameColor, f"Y: {int(depthData.spatialCoordinates.y)} mm", (xmin + 10, ymin + 35), fontType, 0.5, color)
102 cv2.putText(depthFrameColor, f"Z: {int(depthData.spatialCoordinates.z)} mm", (xmin + 10, ymin + 50), fontType, 0.5, color)
103 # Show the frame
104 cv2.imshow("depth", depthFrameColor)
105
106 key = cv2.waitKey(1)
107 if key == ord('q'):
108 break
109 elif key == ord('w'):
110 if topLeft.y - stepSize >= 0:
111 topLeft.y -= stepSize
112 bottomRight.y -= stepSize
113 newConfig = True
114 elif key == ord('a'):
115 if topLeft.x - stepSize >= 0:
116 topLeft.x -= stepSize
117 bottomRight.x -= stepSize
118 newConfig = True
119 elif key == ord('s'):
120 if bottomRight.y + stepSize <= 1:
121 topLeft.y += stepSize
122 bottomRight.y += stepSize
123 newConfig = True
124 elif key == ord('d'):
125 if bottomRight.x + stepSize <= 1:
126 topLeft.x += stepSize
127 bottomRight.x += stepSize
128 newConfig = True
129 elif key == ord('1'):
130 calculationAlgorithm = dai.SpatialLocationCalculatorAlgorithm.MEAN
131 print('Switching calculation algorithm to MEAN!')
132 newConfig = True
133 elif key == ord('2'):
134 calculationAlgorithm = dai.SpatialLocationCalculatorAlgorithm.MIN
135 print('Switching calculation algorithm to MIN!')
136 newConfig = True
137 elif key == ord('3'):
138 calculationAlgorithm = dai.SpatialLocationCalculatorAlgorithm.MAX
139 print('Switching calculation algorithm to MAX!')
140 newConfig = True
141 elif key == ord('4'):
142 calculationAlgorithm = dai.SpatialLocationCalculatorAlgorithm.MODE
143 print('Switching calculation algorithm to MODE!')
144 newConfig = True
145 elif key == ord('5'):
146 calculationAlgorithm = dai.SpatialLocationCalculatorAlgorithm.MEDIAN
147 print('Switching calculation algorithm to MEDIAN!')
148 newConfig = True
149
150 if newConfig:
151 config.roi = dai.Rect(topLeft, bottomRight)
152 config.calculationAlgorithm = calculationAlgorithm
153 cfg = dai.SpatialLocationCalculatorConfig()
154 cfg.addROI(config)
155 spatialCalcConfigInQueue.send(cfg)
156 newConfig = False管道
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。