Script 前向帧
演示

设置
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py源代码
Python
PythonGitHub
1#!/usr/bin/env python3
2import cv2
3import depthai as dai
4
5# Start defining a pipeline
6pipeline = dai.Pipeline()
7
8cam = pipeline.create(dai.node.ColorCamera)
9# Not needed, you can display 1080P frames as well
10cam.setIspScale(1,2)
11
12# Script node
13script = pipeline.create(dai.node.Script)
14script.setScript("""
15 ctrl = CameraControl()
16 ctrl.setCaptureStill(True)
17 # Initially send still event
18 node.io['ctrl'].send(ctrl)
19
20 normal = True
21 while True:
22 frame = node.io['frames'].get()
23 if normal:
24 ctrl.setAutoExposureCompensation(3)
25 node.io['stream1'].send(frame)
26 normal = False
27 else:
28 ctrl.setAutoExposureCompensation(-3)
29 node.io['stream2'].send(frame)
30 normal = True
31 node.io['ctrl'].send(ctrl)
32""")
33cam.still.link(script.inputs['frames'])
34
35# XLinkOut
36xout1 = pipeline.create(dai.node.XLinkOut)
37xout1.setStreamName('stream1')
38script.outputs['stream1'].link(xout1.input)
39
40xout2 = pipeline.create(dai.node.XLinkOut)
41xout2.setStreamName('stream2')
42script.outputs['stream2'].link(xout2.input)
43
44script.outputs['ctrl'].link(cam.inputControl)
45
46# Connect to device with pipeline
47with dai.Device(pipeline) as device:
48 qStream1 = device.getOutputQueue("stream1")
49 qStream2 = device.getOutputQueue("stream2")
50 while True:
51 cv2.imshow('stream1', qStream1.get().getCvFrame())
52 cv2.imshow('stream2', qStream2.get().getCvFrame())
53 if cv2.waitKey(1) == ord('q'):
54 breakPipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。