Object tracker on video
Similar samples:
Demo
Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
PythonGitHub
1#!/usr/bin/env python3
2
3from pathlib import Path
4import cv2
5import depthai as dai
6import numpy as np
7import time
8import argparse
9
10labelMap = ["person", ""]
11
12nnPathDefault = str((Path(__file__).parent / Path('../models/person-detection-retail-0013_openvino_2021.4_7shave.blob')).resolve().absolute())
13videoPathDefault = str((Path(__file__).parent / Path('../models/construction_vest.mp4')).resolve().absolute())
14parser = argparse.ArgumentParser()
15parser.add_argument('-nnPath', help="Path to mobilenet detection network blob", default=nnPathDefault)
16parser.add_argument('-v', '--videoPath', help="Path to video frame", default=videoPathDefault)
17
18args = parser.parse_args()
19
20# Create pipeline
21pipeline = dai.Pipeline()
22
23# Define sources and outputs
24manip = pipeline.create(dai.node.ImageManip)
25objectTracker = pipeline.create(dai.node.ObjectTracker)
26detectionNetwork = pipeline.create(dai.node.MobileNetDetectionNetwork)
27
28manipOut = pipeline.create(dai.node.XLinkOut)
29xinFrame = pipeline.create(dai.node.XLinkIn)
30trackerOut = pipeline.create(dai.node.XLinkOut)
31xlinkOut = pipeline.create(dai.node.XLinkOut)
32nnOut = pipeline.create(dai.node.XLinkOut)
33
34manipOut.setStreamName("manip")
35xinFrame.setStreamName("inFrame")
36xlinkOut.setStreamName("trackerFrame")
37trackerOut.setStreamName("tracklets")
38nnOut.setStreamName("nn")
39
40# Properties
41xinFrame.setMaxDataSize(1920*1080*3)
42
43manip.initialConfig.setResizeThumbnail(544, 320)
44# manip.initialConfig.setResize(384, 384)
45# manip.initialConfig.setKeepAspectRatio(False) #squash the image to not lose FOV
46# The NN model expects BGR input. By default ImageManip output type would be same as input (gray in this case)
47manip.initialConfig.setFrameType(dai.ImgFrame.Type.BGR888p)
48manip.inputImage.setBlocking(True)
49
50# setting node configs
51detectionNetwork.setBlobPath(args.nnPath)
52detectionNetwork.setConfidenceThreshold(0.5)
53detectionNetwork.input.setBlocking(True)
54
55objectTracker.inputTrackerFrame.setBlocking(True)
56objectTracker.inputDetectionFrame.setBlocking(True)
57objectTracker.inputDetections.setBlocking(True)
58objectTracker.setDetectionLabelsToTrack([1]) # track only person
59# possible tracking types: ZERO_TERM_COLOR_HISTOGRAM, ZERO_TERM_IMAGELESS, SHORT_TERM_IMAGELESS, SHORT_TERM_KCF
60objectTracker.setTrackerType(dai.TrackerType.ZERO_TERM_COLOR_HISTOGRAM)
61# take the smallest ID when new object is tracked, possible options: SMALLEST_ID, UNIQUE_ID
62objectTracker.setTrackerIdAssignmentPolicy(dai.TrackerIdAssignmentPolicy.SMALLEST_ID)
63
64# Linking
65manip.out.link(manipOut.input)
66manip.out.link(detectionNetwork.input)
67xinFrame.out.link(manip.inputImage)
68xinFrame.out.link(objectTracker.inputTrackerFrame)
69detectionNetwork.out.link(nnOut.input)
70detectionNetwork.out.link(objectTracker.inputDetections)
71detectionNetwork.passthrough.link(objectTracker.inputDetectionFrame)
72objectTracker.out.link(trackerOut.input)
73objectTracker.passthroughTrackerFrame.link(xlinkOut.input)
74
75# Connect and start the pipeline
76with dai.Device(pipeline) as device:
77
78 qIn = device.getInputQueue(name="inFrame")
79 trackerFrameQ = device.getOutputQueue(name="trackerFrame", maxSize=4)
80 tracklets = device.getOutputQueue(name="tracklets", maxSize=4)
81 qManip = device.getOutputQueue(name="manip", maxSize=4)
82 qDet = device.getOutputQueue(name="nn", maxSize=4)
83
84 startTime = time.monotonic()
85 counter = 0
86 fps = 0
87 detections = []
88 frame = None
89
90 def to_planar(arr: np.ndarray, shape: tuple) -> np.ndarray:
91 return cv2.resize(arr, shape).transpose(2, 0, 1).flatten()
92
93 # nn data, being the bounding box locations, are in <0..1> range - they need to be normalized with frame width/height
94 def frameNorm(frame, bbox):
95 normVals = np.full(len(bbox), frame.shape[0])
96 normVals[::2] = frame.shape[1]
97 return (np.clip(np.array(bbox), 0, 1) * normVals).astype(int)
98
99 def displayFrame(name, frame):
100 for detection in detections:
101 bbox = frameNorm(frame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax))
102 cv2.rectangle(frame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), (255, 0, 0), 2)
103 cv2.putText(frame, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
104 cv2.putText(frame, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
105 cv2.imshow(name, frame)
106
107 cap = cv2.VideoCapture(args.videoPath)
108 baseTs = time.monotonic()
109 simulatedFps = 30
110 inputFrameShape = (1920, 1080)
111
112 while cap.isOpened():
113 read_correctly, frame = cap.read()
114 if not read_correctly:
115 break
116
117 img = dai.ImgFrame()
118 img.setType(dai.ImgFrame.Type.BGR888p)
119 img.setData(to_planar(frame, inputFrameShape))
120 img.setTimestamp(baseTs)
121 baseTs += 1/simulatedFps
122
123 img.setWidth(inputFrameShape[0])
124 img.setHeight(inputFrameShape[1])
125 qIn.send(img)
126
127 trackFrame = trackerFrameQ.tryGet()
128 if trackFrame is None:
129 continue
130
131 track = tracklets.get()
132 manip = qManip.get()
133 inDet = qDet.get()
134
135 counter+=1
136 current_time = time.monotonic()
137 if (current_time - startTime) > 1 :
138 fps = counter / (current_time - startTime)
139 counter = 0
140 startTime = current_time
141
142 detections = inDet.detections
143 manipFrame = manip.getCvFrame()
144 displayFrame("nn", manipFrame)
145
146 color = (255, 0, 0)
147 trackerFrame = trackFrame.getCvFrame()
148 trackletsData = track.tracklets
149 for t in trackletsData:
150 roi = t.roi.denormalize(trackerFrame.shape[1], trackerFrame.shape[0])
151 x1 = int(roi.topLeft().x)
152 y1 = int(roi.topLeft().y)
153 x2 = int(roi.bottomRight().x)
154 y2 = int(roi.bottomRight().y)
155
156 try:
157 label = labelMap[t.label]
158 except:
159 label = t.label
160
161 cv2.putText(trackerFrame, str(label), (x1 + 10, y1 + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
162 cv2.putText(trackerFrame, f"ID: {[t.id]}", (x1 + 10, y1 + 35), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
163 cv2.putText(trackerFrame, t.status.name, (x1 + 10, y1 + 50), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
164 cv2.rectangle(trackerFrame, (x1, y1), (x2, y2), color, cv2.FONT_HERSHEY_SIMPLEX)
165
166 cv2.putText(trackerFrame, "Fps: {:.2f}".format(fps), (2, trackerFrame.shape[0] - 4), cv2.FONT_HERSHEY_TRIPLEX, 0.4, color)
167
168 cv2.imshow("tracker", trackerFrame)
169
170 if cv2.waitKey(1) == ord('q'):
171 breakPipeline
需要帮助?
请前往 Discussion Forum 获取技术支持或提出您可能有的任何其他问题。